You can enter variable strings as an expression.
For example, if you want to add together two integer variables, follow these steps:
to open the PLC"Programmable Logic Controller"
A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Variable Selector
Figure 3-19: Watch Window - Creating Expression


What you can include in a complex expression:
Please note that the DIVIDE SIGN (/) is not interpreted as an operator when used with prefixed variables (e.g. MachineLogic/lastTravelSpeed)
|
Copyright © 2015 Kollmorgen™ |
|